Technical FAQs

Ask a Question

What is the temperature rating of the studs on a QU12L400CL Meter Main unit?

There is no temperature rating on the studs. The lug landing pads where the lugs are attached has been tested for lugs with wire rated or sized for the 75 degrees Celsius table in the N.E.C..

CTA-ID : 2023663
Was this helpful?
What can we do to improve the information ?