Technical FAQs

Ask a Question

What is the interior mounting bag assembly part number for a 100A or 225A NQOD interior?

The part number is 80116-121-50. This bag assembly contains the hardware required to mount the interior in the box, bonding strap, circuit numbers and instruction manuals.


Revised 3/10/04



CTA-ID : 2023230
Was this helpful?
What can we do to improve the information ?