Technical FAQs

Ask a Question

What is the largest branch unit that can go in a 1200A QMB marked #45278-1?

Please refer to Supplementary & Obsolescence Digest 173 page 13-3 where explanations are given about branch capacity as it relates to the various styles panels over the years.

CTA-ID : 2023064
Was this helpful?
What can we do to improve the information ?