Technical FAQs

Ask a Question

I purchased a PK0GTA ground bar kit, and it came with two separate tang lugs and a screw. Should I stack the lugs on top of each other using the one screw to install both?

Yes. The PK0GTA ground bar kit consists of two lugs, both mounted with the same screw.


CTA-ID : 2022906
Was this helpful?
What can we do to improve the information ?