Technical FAQs

Ask a Question

Why does the EZM Main Breaker device, catalog number EZM11200TBU not have the neutral bonded to ground?

Issue:
Product Features

Product Line:
EZM Metering

Environment:
Bonding

Cause:
Application

Resolution:

Bonding or not bonding is the option of the installer based on their application for Service Entrance or not. The EZM main device is bondable in the field and comes with a bag assembly that contains the bus bonding strap used to bond the device. 


CTA-ID : 2022905
Was this helpful?
What can we do to improve the information ?