Technical FAQs

Ask a Question

Why does unit with the V2.0 Powersuite software get an error message indicating problems with the TCP/IP port? The error reads as follows. ``It is impossible to launch the TCP/IP server of configuration. Please check that the protocol TCP/IP well is installed and active on the PC or if another Powersuite application is in course of execution.``

The version V2.0 Powersuite uses TCP/IP protocol. With Windows 98 this driver is not automatically installed, need to install using the Windows 98 CD-Rom.


CTA-ID : 2023204
Was this helpful?
What can we do to improve the information ?