Technical FAQs

Ask a Question

Can RBA800 fuses be used with a 600A HVL switch?

Yes they can, but the end user must know not to install refills above 540E. The RBA800 fuse holders can be fused up to 720E, but the fusing must not exceed the interrupting current of the switch which is 600A.

CTA-ID : 2023209
Was this helpful?
What can we do to improve the information ?