Technical FAQs

Ask a Question

Coil 31104-400-50. Why is it used on all the voltages?

It is a DC coil fed by a Control Module which is fed by the 120v secondary of a control transformer . The coil is the same regardless of the control voltage.


CTA-ID : 2035282
Was this helpful?
What can we do to improve the information ?