Technical FAQs

Ask a Question

What is the replacement plug-in opening door, for plug-in busway, on I-Line I busway, Series 3 and 4?<br /><br />

1 each of 4520204050 (door) and 2 each of 4511200401 (hinge spring). These are the same for the older I-Line plug-in busway from 800A to 5000A.

CTA-ID : 2022452
Was this helpful?
What can we do to improve the information ?