Technical FAQs

Ask a Question

What is the minimum ampere rating of a branch circuit breaker for the QO and Homeline load centers?

Issue:
Product Availability

Product Line:
QO and Homeline Load Centers

Environment:
Branch Breakers

Cause:
Application

Resolution:
The minimum ampere rating for a branch breaker for the QO load centers is 10amps. The minimum ampere rating for a branch breaker for the Homeline load centers is 15amp. SEE THE CURRENT DIGEST FOR CATALOG NUMBERS.


CTA-ID : 2022895
Was this helpful?
What can we do to improve the information ?