Technical FAQs

Ask a Question

What is the catalog number for the Control Wire Termination Kits for a MA or MAL breaker?

AL900MAT which accepts 3-#3/0 AWG to 500 kcmil per phase or AL1000MAT which accepts 4-#1/0 AWG to 350 kcmil per phase.

CTA-ID : 2023202
Was this helpful?
What can we do to improve the information ?