Technical FAQs

Ask a Question

Customer has part number 26858, M9 RCBO and wants to know the gauge wire for the neutral and ground wires.

Neutral cable section :
up to 32A = 2.5 mm?
for 40 and 45A =4 mm? (40A not sold under Square D brand)
Ground cable section :
0.75 mm?


CTA-ID : 2022880
Was this helpful?
What can we do to improve the information ?