Technical FAQs

Ask a Question

Are optional lugs available for a DJM circuit breaker used in an EZML332400 branch device?

An optional field installed lug, catalog number 32510, accepts (2) #2/0 AWG - 350 kcmil copper or (2) #2/0 AWG - 500 kcmil aluminum conductors. The standard lug, catalog number 32508, accepts (1) #2 AWG - 600 kcmil copper or (1) #2 AWG - 500 kcmil aluminum conductor.
NOTE: The optional lug referenced is for the DJM circuit breaker only. It is not an optional lug for the branch neutral bar.


CTA-ID : 2023321
Was this helpful?
What can we do to improve the information ?