Technical FAQs

Ask a Question

What boots are suggested with a 9001SKR*U pushbutton operators?

Suggested boots are as follows:
1) For multispeed operators, the 9001 KU37 is recommended.
2) For momentary single speed operators, the 9001 KU1 is recommended.
3) For maintained single speed operators the 9001 KU27 is recommended.


CTA-ID : 2022792
Was this helpful?
What can we do to improve the information ?