Technical FAQs

Ask a Question

Do the Integral self-protected starters provide automatic reset?

No, however there is a remote reset module which can be wired in conjunction with a timer to provide this function on the 32 and 63 amp versions.


CTA-ID : 2020598
Was this helpful?
What can we do to improve the information ?