Technical FAQs

Ask a Question

Do we have any enclosures for a QBL32250?

Issue:
Selection

Product Line:
Circuit Breaker Enclosures

Cause:
Selection

Resolution:
There is no separate enclosure offered for a 250A Q-Frame PowerPact circuit breaker. The maximum is 225A.
The Q23225NS, Q23225NF and Q23225NRB enclosures are rated up to 225A and accept 2P or 3P Q-Frame PowerPact circuit breakers.
The Q22200NS and Q22200NRB enclosures are rated up to 200A and accept 2P Q-Frame PowerPact circuit breakers. 


CTA-ID : 2023042
Was this helpful?
What can we do to improve the information ?