Technical FAQs

Ask a Question

What is the Nema rating for the XVB indicating beacons?

The protection ratings are IP 65 and Type 1, 4X (indoor) & 12.


CTA-ID : 2023036
Was this helpful?
What can we do to improve the information ?