Technical FAQs

Ask a Question

What is the AIR rating of an FCL breaker at 480v ?

It is 65 kA at 480 Vac. At 240 Vac it is 100 kA .


CTA-ID : 2022875
Was this helpful?
What can we do to improve the information ?