Technical FAQs

Ask a Question

What is the maximum amp rating offered for an NQOD panel ?

It is available at 600a max , single or 3 phase ; with main breaker factory assembled only or with main lugs factory assembled or ready-to-assemble

CTA-ID : 2023178
Was this helpful?
What can we do to improve the information ?