Technical FAQs

Ask a Question

When using a the Class 9421 door mounted circuit breaker operating mechanism, does the breaker have to be turned OFF before opening the enclosure door?

Yes, however there is a defeat mechanism which will allow for opening of the enclosure door while the switch is in the ON position.

CTA-ID : 2020341
Was this helpful?
What can we do to improve the information ?