Technical FAQs

Ask a Question

What are the tightening torque requirements for the Class 8536 Type SC NEMA size 1 starter? <br />

Line and load power terminals - 20 lbs.-in.
Control coil terminals - 9 -12 lbs.-in.
Auxiliary contact terminals - 18 - 21 lbs.-in.
Overload relay control contact module terminals - 9 -12 lbs.-in.
Thermal unit fastening screws - 18 - 21 lbs.-in.


CTA-ID : 2020316
Was this helpful?
What can we do to improve the information ?