Technical FAQs

Ask a Question

Why does the rFr parameter not come up as a possible assignment in the dO code of the I/O menu when trying to set the analog output to identify motor frequency of the ATV31?

The VVDED303042USR6/04 Altivar 31 programming manual is incorrect.
The selection of motor frequency appears as OFr rather than rFr.

CTA-ID : 2022504
Was this helpful?
What can we do to improve the information ?