Technical FAQs

Ask a Question

Is there a protective boot for the Class 9999 Type SA2, SA10, SC2 or SC22 NEMA 1 rectangular operators?

No, these control stations are intended for use in NEMA 1 applications only.


CTA-ID : 2023030
Was this helpful?
What can we do to improve the information ?