Technical FAQs

Ask a Question

What is the contact arrangement shown as 2 NO 2 NC on a 9007 C62B2?

The contacts are 2 double pole double throw form ZZ contacts and use a snap action contact block. Polarity must be the same on each double pole double throw contact.


CTA-ID : 2022831
Was this helpful?
What can we do to improve the information ?