Technical FAQs

Ask a Question

What is the NEMA enclosure rating of the 9001SKYP2,-4, -6, -8, and -10 pendant?

Issue:
What is the NEMA enclosure rating of the 9001SKYP2,-4, -6, -8, and -10 pendant?

Product Line:
Harmony Pendant Stations

Environment:
All products

Cause:
Product Features


Resolution:
It is rated for NEMA 1, 3, 4, 4X, and 13.


CTA-ID : 2020131
Was this helpful?
What can we do to improve the information ?