Technical FAQs

Ask a Question

What operating handles should be used with the Class 9422 Type TF* disconnect switches?

Use either the 9422A1 or 9422A2 handle assembly as the 9422A3 and 9422A4 handle assemblies are to short and not recommended.


CTA-ID : 2023018
Was this helpful?
What can we do to improve the information ?