Technical FAQs

Ask a Question

What is the terminal lug data for a QO342MQ225RB load center? <br />

Main wire size is a #4-300 Al/Cu AWG/kcmil wire. (this is also marked on the Load center wiring diagram)


CTA-ID : 2023014
Was this helpful?
What can we do to improve the information ?