Technical FAQs

Ask a Question

What is the maximum branch breaker that can be used in the load center interior of a SU3040D400CB?

200amp maximum.(please see wiring diagram on the device)


CTA-ID : 2023013
Was this helpful?
What can we do to improve the information ?