Technical FAQs

Ask a Question

What are the dimensions for 7.5hp and the 10hp 208V enclosed ATS48 units?

The dimensions for Size A enclosure listed for 3-5hp 208V should also apply for the 7.5hp and 10hp, 208V units. There is a typo in the manual. The dimensions are 15.011`` (381.3mm) deep, 33.433`` (849.2mm) tall and 24.660`` (627.1mm) wide.

CTA-ID : 2023169
Was this helpful?
What can we do to improve the information ?