Technical FAQs

Ask a Question

What is the replacement base and cover for a XVAL or XVAC?

Issue:
What is the replacement base and cover for a XVAL or XVAC?

Product Line:
Harmony Tower Lights

Environment:
All Products

Cause:
Product selection

Resolution:
XVAC211 is replacement base and cover for all XVAL or XVAC units. The XVAC211 is now obsolete. It can be replaced with an XVEC21, IP 42, and if needed a gasket kit XVEZ082, IP 54. The XVEC21 cannot be direct mounted. It must be mounted on a support tube with mounting base or conduit adapter, XVAC00.


CTA-ID : 577
Was this helpful?
What can we do to improve the information ?