Technical FAQs

Ask a Question

What is the maximum amperage breaker that can be put in the 200 amp loadcenter in the CU12L400CB ?

125 amp is maximum amperage breaker that can be put in the loadcenter in the CU12L400CB.


CTA-ID : 2023004
Was this helpful?
What can we do to improve the information ?