Technical FAQs

Ask a Question

Does the XALK194 E-stop control station have a maintained contact?

Issue:
Does the XALK194 E-stop control station have a maintained contact?
Product Line:
22mm Control Stations and Enclosures                   
Environment:
XAL 22MM Control Stations
Cause:
Clarify if the operator or contact block is maintained.       
Resolution:                                                                 
The contact is momentary, but the operator is a maintained push pull mushroom button. This will hold the contact open when the button is depressed.
 
Was this helpful?
What can we do to improve the information ?