Technical FAQs

Ask a Question

Does a ``TVS2EMA`` series include a ``surge counter with time and date stamping, that is PC downloadable via RS-232 ?

Issue:
Surge counter w/ time and date stamping

Product Line:
Surge Protection Devices

Environment:
EMA

Cause:
Product feature

Resolution:
The Surge Logic EMA has a surge counter but not with networking capabilities. At present a visual product display is the only way
to check the surge counter.



CTA-ID : 2023265
Was this helpful?
What can we do to improve the information ?