Technical FAQs

Ask a Question

What is the AIC Rating for a LX36400G at 480V?

AIR is 65kA @ 480Vac. See selection table in the breaker section of the Digest.


CTA-ID : 2023257
Was this helpful?
What can we do to improve the information ?