Technical FAQs

Ask a Question

Do the F-Line LR9F**** overload relays provide phase unbalance / phase failure protection?

Product Line:
 
Tesys F line Contactors and Accessories
 
Resolution:
 
Yes the LR9F**** Solid State Overload Relays provide protection against motor overload, phase failure or phase unbalance of 30% or greater and locked rotor conditions.


CTA-ID : 2022998
Was this helpful?
What can we do to improve the information ?