Technical FAQs

Ask a Question

What is the difference between 9007MS10S000685 and 9007MS10S000654 limit switch with a 4-pin dc connector?

Both have a 4-pin connectors but the keyways are different. 9007MS10S000685: booted top plunger, form C - SPDT silver contacts, no cable, side entry, with 4 pin DC connector with key way oriented 180 deg. from standard. This arrangement will allow a 90 degree female connector to be connected, so that it faces downward if looking at the limit switch`s nameplate.




CTA-ID : 2022994
Was this helpful?
What can we do to improve the information ?