Technical FAQs

Ask a Question

Are the Quick Start Procedure steps in the ATS48 manual correct? It says in step 4 to set parameter In and then in step 5 it says apply control power to CL1 & CL2?

These two steps are out of order. To set a parameter it is necessary to apply control power first.

CTA-ID : 2022993
Was this helpful?
What can we do to improve the information ?