Technical FAQs

Ask a Question

Customer is trying to order a 7001KEO11 with 2 n.c. and 2 n.o. contacts.

Order a 7001KEO22, specify the system voltage and pick up or drop out voltage, and if both are required specify which is more important.

The crane control portion of this business is now owned by E. C. & M. Call 1-800-240-1230 for technical support.

CTA-ID : 2006149
Was this helpful?
What can we do to improve the information ?