Technical FAQs

Ask a Question

What is the part number of the Nema 1 enclosure for a 1200 amp 3 pole breaker NX breaker w/ shunt trip and solid neutral?

We do not have a Nema 1 enclosure for the NXL breaker. The only enclosure is a Nema 12 enclosure part number NA1200AWK.

CTA-ID : 2022990
Was this helpful?
What can we do to improve the information ?