Technical FAQs

Ask a Question

Are cover mounted control stations such as Hand-Off-Auto, Start - Stop pushbuttons, etc. available for the Class 9991 Type DPG4 enclosure?<br />

No, there is no cover knockout for control stations or pilot lights. Suggest the use of 30 mm operators mounted in the side of the box or a separate mount control station.


CTA-ID : 2023350
Was this helpful?
What can we do to improve the information ?