Technical FAQs

Ask a Question

What is the part number for the IGBT assembly with gate driver board ATV66C19N4?

There are two kits. One kit for Design A. Another Kit for designs B & C. Be sure to correctly identify the correct kit.

For Design A, the part number is VZ3IM1500M1206 - This kit includes four snubber board, two gate driver boards, two IGBT power module, thernstrate thermal interface material and two control wire assemblies.    Design A was manufactured up until the end of May 1998.  These drive controllers DO NOT have a 1 as the seventh digit of the serial number.

For Designs B & C, the part number is VZ3IM2400M1202- This kit includes four snubber board, two gate driver boards, two IGBT power module, thernstrate thermal interface material and two control wire assemblies.    Design B was manufactured after May 1998.  These drive controllers DO have a 1 as the seventh digit of the serial number.


CTA-ID : 2023348
Was this helpful?
What can we do to improve the information ?