Technical FAQs

Ask a Question

How is an HOMT2020230 quad tandem breaker configured?

The outer poles are 20A single pole circuit breakers and the inner 2 poles are a 30A double pole common trip circuit. The catalog numbering system is typical for the other quad tandems.


CTA-ID : 2023341
Was this helpful?
What can we do to improve the information ?