Technical FAQs

Ask a Question

What is the temperature rating of the lugs for the NQOD panel?

The lugs are rated for 75 degree C wire.


CTA-ID : 2023116
Was this helpful?
What can we do to improve the information ?