Technical FAQs

Ask a Question

Are the support couplings provided with each section of underfloor duct?

Issue:
Selection

Product Line:
Wire Management

Environment:
NFPA 70 Art.354, Art. 356; UL884; UL209

Cause:
Changes to usage of a space can drive the need to modify existing underfloor duct installations.

Resolution:
The underfloor duct and its associated service fittings and accessories are now obsolete and no longer available.

Support couplings were ordered separately.


CTA-ID : 2022976
Was this helpful?
What can we do to improve the information ?