Technical FAQs

Ask a Question

Am hearing a loud humming noise on a QO350 breaker in a 3 phase panel board. Is this normal?

Some humming is normal in most breakers under load. The magnetic field may cause metal parts in them to vibrate. Unless the noise is excessive, it is nothing to worry about.


CTA-ID : 2023339
Was this helpful?
What can we do to improve the information ?