Technical FAQs

Ask a Question

Does the XACA2073 come with contacts?

Issue:
Does the XACA2073 come with contacts?

Product Line:
Pendant Station   

Environment:
XAC Standard Duty Pistol Grips

Cause:
Clarify if contacts are included with the part number.        

Resolution:                                                                 
XACA2073 has 2 normally open (staggered) contacts per operator.
 
Was this helpful?
What can we do to improve the information ?