Technical FAQs

Ask a Question

Are there optional copper compression lugs available for HD, HG, HJ, HL circuit breakers?

Yes, there are 2 different lugs available. Catalog number CYA060HD is a set of 3 lugs with a wire range of 1 -#6 to #1/0 AWG CU . Catalog number CYA150HD is a set of 3 lugs with a wire range of #4 to 2/0 AWG CU.


CTA-ID : 2023091
Was this helpful?
What can we do to improve the information ?