Technical FAQs

Ask a Question

What is the part number for the optional line reactor mounted internally on the 1-25hp ATV58 Econoflex drives?

The reactor is made by TCI and the TCI part number is KLR45BTB. The Square D part number is 26155-232-45 but the order has to be forced on Seneca.


CTA-ID : 2022959
Was this helpful?
What can we do to improve the information ?