Technical FAQs

Ask a Question

What is the Terminal Lug Data for a DJM circuit breaker used in an EZML311400 branch device?

The standard lug, catalog number 32508, accepts (1) #2 AWG - 600 kcmil copper or (1) #2 AWG - 500 kcmil aluminum conductor.


CTA-ID : 2023325
Was this helpful?
What can we do to improve the information ?