Technical FAQs

Ask a Question

What is the Terminal Lug Data for a DJM circuit breaker used in an EZML332400 branch device?

Issue:
Wire Range 

Product Line:
EZM Metering

Environment:
Tenant breaker wiring 

Cause:
Terminal lug data

Resolution:

The standard lug for the DJM tenant circuit breaker, is catalog number 32508 and accepts (1) #2 AWG - 600 kcmil copper or (1) #2 AWG - 500 kcmil aluminum conductor.


CTA-ID : 2023324
Was this helpful?
What can we do to improve the information ?